I cannot log on to the FactoryTalk Directory

Before the RSSecurity database is imported into a
FactoryTalk Directory
, log on to that directory. If problems arise logging on to the
FactoryTalk Directory
, it might be because:
  • Logging on to the wrong
    FactoryTalk Directory
    . Verify the Network Directory or Local Directory where to import the RSSecurity database.
  • The
    FactoryTalk Directory
    is not configured on the computer, if the computer is running
    FactoryTalk Automation Platform
    2.00 (CPR 7).
  • The administrator account on the
    FactoryTalk Directory
    is disabled.
  • The physical computer acting as the
    FactoryTalk Directory
    server was replaced, but the name of the new server computer was not changed so
    FactoryTalk Directory
    clients think they are still connected, but they are not.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal