FactoryTalk Live Data Test Client Help
How do I open
FactoryTalk Live Data Test Client
?
Go to
Rockwell Software > FactoryTalk Live Data Test Client
.Use
FactoryTalk® Live Data Test Client
to test the communications network for your FactoryTalk
system. FactoryTalk Live Data Test Client
reads and writes data items contained in:- FactoryTalkdata servers, such asFactoryTalk LinxorFactoryTalk View SE
- OPC-DA 2.0 compliant data servers, includingRSLinx Classicand third-partyOPCDA servers
FactoryTalk Live Data Test Client
can monitor each data item individually or as part of a custom group. Activate, deactivate, or change the read and write settings of data items and groups to verify their values are correctly transferred across the network.Simulate the network traffic generated by an HMI system by setting a group to run in HMI Emulation mode.
FactoryTalk Live Data Test Client
automatically switches from one group of data items to the next, simulating how operators may frequently change graphic displays.Save
FactoryTalk Live Data Test Client
configurations to reuse data item and group settings in future tests.Provide Feedback