LCD instructions
Use LCD instructions to read or write data to or from a module using signals sent to a device that is physically connected to a programmable logic controller.
Instruction | Description |
|---|---|
Displays a string or number on an LCD screen. Micro810 only. | |
Reads the Key status on the optional remote LCD module when the user display is active. L20E only. | |
Sets the remote LCD backlight parameters in a user program. | |
Displays user-defined messages for the remote LCD. | |
Reads the Key status on the optional LCD module when the user display is active. Micro810 only. |
Provide Feedback