KEY_READ (read keys on LCD)
The KEY_READ instruction reads the Key status on the optional LCD module when the user display is active.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro810
controller.KEY_READ

Parameter | Parameter Type | Data Type | Description |
|---|---|---|---|
Enable | Input | BOOL | Enables the instruction block.
|
CKYL | Output | BOOL | TRUE: ESC key pressed for more than 2 seconds. |
EKYL | Output | BOOL | TRUE: OK key pressed for more than 2 seconds. |
CKY | Output | BOOL | TRUE: ESC key pressed. |
EKY | Output | BOOL | TRUE: OK key pressed. |
UKY | Output | BOOL | TRUE: Up key pressed. |
DKY | Output | BOOL | TRUE: Down key pressed. |
LKY | Output | BOOL | TRUE: Left key pressed. |
RKY | Output | BOOL | TRUE: Right key pressed. |
KEY_READ examples
KEY_READ function block diagram example

KEY_READ ladder diagram example

KEY_READ structured text example

(* ST Equivalence: *) KEY_READ_1(KEYENABLE) ; KEY_EKYL := KEY_READ_1.EKYL ; KEY_CKY := KEY_READ_1.CKY ; KEY_EKY := KEY_READ_1.EKY ; KEY_UKY := KEY_READ_1.UKY ; KEY_DKY := KEY_READ_1.DKY ; KEY_RKY := KEY_READ_1.RKY ; KEY_LKY := KEY_READ_1.LKY ;
Provide Feedback