File/Shift instructions
Use File/Shift instructions to modify the location of data.
Instruction | Description |
|---|---|
Shifts a bit in an array element to the left. | |
Shifts a bit in an array element to the right. | |
Loads 8-bit, 16-bit, 32-bit, or 64-bit data into a user-created array called a FIFO stack. | |
Unloads 8-bit, 16-bit, 32-bit, or 64-bit data from a user-created array called a FIFO stack. The data unloads in the same order as loaded using the FFL instruction. | |
Loads 8-bit, 16-bit, 32-bit, or 64-bit data into a user-created array called a LIFO stack. | |
Unloads 8-bit, 16-bit, 32-bit, or 64-bit data from a user-created array called a LIFO stack. The data unloads in the same order as loaded using the LFL instruction. | |
For 32-bit integers, rotates integer bits to the left. | |
For 32-bit integers, rotates integer bits to the left. | |
For 32-bit integers, moves integers to the left and places 0 in the least significant bit. | |
For 32-bit integers, moves integers to the right and places 0 in the most significant bit. | |
Manages a stack of integer values. |
Provide Feedback