SHR (shift right)
The SHR instruction shifts the 32 bits of an integer to the right and replicates the leftmost bit (significant bit) to fill the vacant bits.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the Micro810, L20E, L50E, and L70E controllers.
SHR

SHR

Parameter | Parameter Type | Data Type | Description |
|---|---|---|---|
EN | Input | BOOL | When set to true, the instruction is enabled.
|
IN | Input | DINT | Any integer value. |
NbS | Input | DINT | Number of 1 bit shifts (in set [1..31]). |
SHR | Output | DINT | Right shifted value. There is no effect if NbS <= 0. If a value of 0, replaces the most significant bit. |
ENO | Output | BOOL | Enables output. Applies to ladder diagram programs. |
SHR examples
SHR function block Diagram example

SHR ladder diagram example

SHR structured text example

(* ST Equivalence: *) result := SHR (register,1); (* register = 2#1100_1101_0011_0101 *) (* result = 2#0110_0110_1001_1010 *)
Results

Provide Feedback