Advanced Math instructions
The Advanced Math instructions include the following:
Instruction | Description |
|---|---|
Differentiates a real value over a defined cycle time. | |
Calculates the Real value of a base number raised to the power of the Integer exponent. | |
Calculates the value of a Real number raised to a power of the Real exponent. | |
Integrates a real value during the defined cycle time. | |
Calculates the logarithm (base 10) of a Real value. | |
Calculates random integer values from a defined range. | |
Calculates the square root of a Real value. |
Provide Feedback