Axis - General tab
Configure the motion settings for the
Micro800
controllers that support motion. After adding an axis to the controller project, use the Axis<x> - General
configuration page to:- Change the axis name.
- Specify thePTO channelthat is used to support axis positioning.
- EnableDrive enable outputto check the output status of the servo drive and set theServo On Output Enableflag.
- EnableDrive ready inputto check the input status of the servo drive and set theServo Ready Input Enableflag.
- EnableIn-position inputto monitor the input status so that the motion engine can tell when the MC_MoveAbsolute and MC_MoveRelative function blocks are completed.
- EnableTouch probe inputto read the input wiring information from the input hardware device.
Setting | Description |
|---|---|
Axis name | Specifies the axis name. The axis name must be unique and does not duplicate with an existing variable name, data type, or reserved word. Axis naming conventions are as follows:
|
PTO channel | Lists the PTO channels available for the axis. The Micro800 controllers that support motion uses PTO to control axis positioning.Each axis is mapped to a PTO channel. By default, the PTO channel value depends on the order that you create the axis. For example,
For more information, see Micro830, Micro850, and Micro870 Programmable Controllers User Manual - 2080-UM002_-EN-E. |
Pulse output | Identifies the pulse output string that is assigned based on the PTO channel selection. The string is read-only.When you select <unassigned> for the PTO channel list, the wiring information is blank.For more information, see Micro830, Micro850, and Micro870 Programmable Controllers User Manual - 2080-UM002_-EN-E. |
Direction output | Identifies the direction output wiring information of the PTO channel that is assigned to the axis. Direction output is read-only and is assigned based on the PTO Channel selection.When you select <unassigned> for the PTO channel , the wiring information is blank. |
Drive enable output | Makes the drive output settings available or not. The settings are available by default. The MC_Power function block controls the output and the MC_Stop function block resets the output. When Drive enable output is selected, the Servo On Output Enable flag is set. |
Drive enable output - Output | Lists the available digital output variables. |
Drive enable output - Active level | Lists the active levels for the drive enable output variable. Options are High and Low . The default setting is High . |
Drive ready input | Makes the drive ready input settings available or not for the servo drive. The settings are available by default. When Drive ready input is selected, the Servo Ready Input Enable flag is set.The check for the servo drive input starts when the MC_Power function block is active and Drive enable output is selected.The MC_Power instruction has a timeout value of 2 minutes. If the timeout period elapses and the value of Drive ready input is False, the MC_Power instruction returns an error. |
Drive ready input - Input | Lists the available digital input variables for the servo drive. |
Drive ready input - Active level | Lists the active levels for the input variable of the servo drive. Options are High and Low . The default setting is High . |
In-position input | Makes the in-position input settings available or not. The settings are not available by default. When In-position input is selected, a port monitors the axis position using the in-position Input variable.The motion engine monitors the input to determine when the MC_MoveAbsolute and MC_MoveRelative function blocks are completed. |
In-position input - Input | Lists the digital input variables for in-position input monitoring. |
In-position input - Active level | Lists the active levels for the in-position input variable. Options are High and Low . The default setting is High . |
Touch probe input | Makes the touch probe input settings available or not. The settings are not available by default. When Touch probe input is selected, Input displays the read-only wiring information, and Active level is available for configuration.The MC_TouchProbe function block uses the input. |
Touch probe input - Input | Shows the read-only input wiring information for the touch probe input, which is assigned based on the input hardware device. |
Touch probe input - Active level | Specifies the active level for the touch probe Input variable. Options are High and Low . The default setting is High . |
Provide Feedback