MC_MoveRelative (motion control move relative)
The MC_MoveRelative instruction commands a controlled motion of a specified distance relative to the actual position at the time of the execution.
Operation details:
- Because the motion direction for MC_MoveRelative is determined by the current position and the target position, the sign of the Velocity is ignored.
- MoveRelative completes with Velocity zero if it is not overridden by another function block.
- If MC_MoveRelative is issued when theMicro800controller axis state is Standstill and the relative distance to move is zero, the execution of the function block is immediately reported as Done.
- For aMicro800controller, the sign of the input Velocity for MC_MoveRelative is ignored because the motion direction is determined by the Current position and the Target position.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the L50E and L70E controllers that support motion control.
MC_MoveRelative

MC_MoveRelative operation
Parameter | Parameter Types | Data Types | Descriptions |
|---|---|---|---|
EN | Input | BOOL | Instruction block enable.
Applies only to ladder diagram programs. |
Execute | Input | BOOL | Indicates when to start motion.
|
Distance | Input | REAL | Relative distance for the motion (in technical unit [u]). |
Velocity | Input | REAL | Value of the maximum velocity (not necessarily reached) [u/s]. Because the motion direction is determined by input Position, the sign of Velocity is ignored by the function block. The maximum velocity might not be reached when Jerk = 0. |
Acceleration | Input | REAL | Value of the acceleration (increasing energy of the motor) [u/s 2 ]. |
Deceleration | Input | REAL | Value of the deceleration (decreasing energy of the motor) [u/s 2 ]. |
Jerk | Input | REAL | Value of the Jerk [u/s 3 ]. |
BufferMode | Input | SINT | This parameter is not used. |
ENO | Output | BOOL | Enable output. Applies only to ladder diagram programs. |
Axis | Output | AXIS_REF | Axis output is read-only in ladder diagram programs. |
Done | Output | BOOL | TRUE: Commanded distance reached. When the in-position input is enabled for an axis, the in-position signal must be set to active before Done = True. |
Busy | Output | BOOL |
|
Active | Output | BOOL | TRUE: Indicates that the instruction block has control on the axis. |
CommandAborted | Output | BOOL | TRUE: Command was overridden by another command, or Error Stop. |
Error | Output | BOOL | Indicates that an error occurred.
|
ErrorID | Output | UINT | A unique numeric that identifies the error. The errors for this instruction are defined in Motion control function block error IDs. |
MC_MoveRelative examples
MC_MoveRelative function block diagram example

MC_MoveRelative ladder diagram example

MC_MoveRelative structured text example

MC_MoveRelative result example


Provide Feedback