MC_TouchProbe (motion control touch probe)
The MC_TouchProbe instruction records an axis position at a trigger event.
Operation details:
- If the window direction (first position to last position) is in the opposite direction of the motion direction, the touch probe window does not activate.
- If the window setting (FirstPosition or LastPosition) is not valid, the MC_TouchProbe function block reports an error.
- If a second instance of the MC_TouchProbe function block is issued on the same axis, and the first function block instance is in a Busy state, the second function block instance reports an error.
- Only one MC_TouchProbe function block instance should be issued to one axis.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the L50E and L70E controllers that support motion control.
MC_TouchProbe

Parameter | Parameter Type | Data Type | Description |
|---|---|---|---|
EN | Input | BOOL | Instruction block enable.
Applies only to ladder diagram programs. |
AxisIn | Input | AXIS_REF FB_AXIS_REF | Use the AXIS_REF data type to define the parameters for AxisIn. For a feedback axis, use the FB_AXIS_REF data type to define the parameters for AxisIn. |
TriggerInp | Input | USINT | Not supported currently. Configure input trigger in the axis configuration. |
Execute | Input | BOOL |
|
WindowOnly | Input | BOOL | TRUE: Only use the window to accept trigger events. Motion resolution is limited to the Motion Engine interval configured by the user. For WindowOnly TouchProbe functionality, there is a maximum response time delay that is equal to the Motion Engine interval for both FirstPosition and LastPosition activation. The maximum possible lag in the triggering position (both FirstPosition and LastPosition) can be calculated by (Motion Engine interval x moving velocity). |
FirstPosition | Input | REAL | Start position of the window from where trigger events are accepted (in technical units [u]). Value included in window. |
LastPosition | Input | REAL | Stop position of the window from where trigger events are not accepted (in technical units [u]). Value included in window. |
ENO | Output | BOOL | Enable output. Applies only to ladder diagram programs. |
Axis | Output | AXIS_REF | Axis output is read-only in ladder diagram programs. |
TriggerInput | Output | USINT | Not supported currently. |
Done | Output | BOOL | TRUE: Trigger event was recorded. |
Busy | Output | BOOL | TRUE: The function block is not finished. |
CommandAborted | Output | BOOL | TRUE: The command was overridden by the MC_Power(OFF), or Error Stop function block. |
Error | Output | BOOL | Indicates that an error occurred.
|
ErrorID | Output | UINT | A unique numeric that identifies the error. The errors for this instruction are defined in Motion control function block error IDs. |
RecordedPosition | Output | REAL | Position where trigger event occurred (in technical units [u]). Motion is an open-loop motion. The axis position at the time the trigger event occurs. If the axis motion is an open-loop motion, the commanded position (not an actual position) at the time the trigger event occurs, if there is no motion delay between the drive and the motor. |
Motion Signals | PTO0 | PTO1 | PTO2 |
|---|---|---|---|
PTO pulse | Output_0 | Output_1 | Output2 |
PTO direction | Output_3 | Output_4 | Output_5 |
Lower (Negative) Limit switch | Input_0 | Input_4 | Input_8 |
Upper (Positive) Limit switch | Input_1 | Input_5 | Input_9 |
Absolute Home switch | Input_2 | Input_6 | Input_10 |
Touch Probe Input switch | Input_3 | Input_7 | Input_11 |
MC_TouchProbe examples
MC_TouchProbe function block diagram example

MC_TouchProbe ladder diagram example

MC_TouchProbe structured text example

Results


Provide Feedback