Motion Event instructions
Use the Motion Event instructions to program and design the motion of a particular axis.
TIP:
- Administrative instructions support both PTO motion and Feedback motion.
- The motion control instructions that support a FBAxis are: MC_ReadActualPosition and MC_ReadActualVelocity.
Instruction | Description |
|---|---|
Cancells Motion function blocks that are connected to trigger events. | |
Records an axis position at a trigger event. |
Provide Feedback