Motion overview
In
FactoryTalk Design Workbench
, Micro800
controllers support motion by using high-speed pulse-train outputs (PTO) for a control axis or a high-speed counter plug-in for a feedback axis.Configuration for an axis includes Limits, Dynamics, and Homing. A control axis is programmed using motion instructions such as MC_MoveRelative. The axis status is available as a global AXIS_REF variable and by using motion instructions such as MC_ReadStatus. The number of supported PTO axes depends on the
Micro800
controller type in the project. The status for the motion engine, axes status, and control information data are available in the global variables.
TIP:
- You must configure the motion settings for the controllers that support motion.
- TheFBAxisoption is available when a 2080-MOT-HSC plug-in module is part of the controller configuration and is enabled with the feedback axis.
Configure PTO motion settings for a
Micro800
controller by doing one of the following actions:- Using the configuration pages available from thePTO Motionnode in theControllertree.
- Creating controller programs using the motion control instructions.
The following section introduces the global variable data types for motion:
- _MOTION_DIAG: A global variable structure data type that contains the status and control information for the motion engine. The variables apply to all axes that are assigned to the controller.
- AXIS_REF: A global variable structure data type that contains the status and control information for an axis of motion.
- FBAXIS_REF: A global variable structure data type that contains status and control information for an FBAxis.
For more information about controller inputs and outputs, see Micro830, Micro850, and Micro870 Programmable Controller User Manual (publication 2080-UM002).
Controller Catalog Number | Number of Control Axes | Maximum Number of Feedback Axes | Number of Inputs | Number of Outputs |
|---|---|---|---|---|
2080-L50E-24QBB | 2 | 3 | 14 | 10 |
2080-L50E-24QVB | 2 | 3 | 14 | 10 |
2080-L50E-48QBB | 3 | 4 | 28 | 20 |
2080-L50E-48QVB | 3 | 4 | 28 | 20 |
2080-L70E-24QBB | 2 | 3 | 14 | 10 |
2080-L70E-24QBBN | 2 | 3 | 14 | 10 |
Provide Feedback