Export data log files from the controller to the local drive
Use the
Manage data logs
button on the Data Log configuration page to export data log files from the controllers to the local drive. Export data log files to save backups in case of an unexpected data loss or to free up space on the SD memory card.By default, data log files are exported to the Downloads folder with the following file name:
- DataLog_<yyyymmdd>_<hhmmss>.m8a
- DataLog_<yyyymmdd>_<hhmmss>.xlsx
To export data log files from the controller to the local drive
- Export the data log file by doing one of the following:
- Select
to export an XLSX file. - Select
to export a M8A file.Use the Settings page from theFilemenu to specify whether to reserve the folder structure of the data log files or export all data logs to one TXT file.
- (optional) InExport, select the export path and enter the file name as needed.
- SelectSave.
Provide Feedback