Fetch data logs
Use
on the
on the <controller-name>: Manage data logs
page to do the following actions:- Fetch data logs for a specified time range from the memory card.
- Fetch data logs for a specified time range from the computer when the controller is offline.
TIP:
- If you fetch data log files when the controller is inRunmode, performance might be affected and the operation might take longer.
- The fetching behavior only applies to data log files. The Header file is regenerated based on the data set configuration.
Prerequisites
- The controller is online.
To fetch data logs
- InProject Organizer, double-click the controller to open the controller application workspace.
- In theControllertree, selectData Log.
- On theData Logconfiguration page, selectManage data logs.
- On the<controller-name>: Manage data logspage, select
to fetch the data log. - Choose the date range for exporting data logs from the controller.
- (optional) When data logs for a particular period exist in the current project, select:
- No, skipto skip fetching data logs for the period and use the data logs in the current project.
- Yes, overwriteto fetch the data logs to overwrite the existing data logs for the period in the memory card or in the computer.
Provide Feedback