Data Log configuration page
The
Data Log
configuration page is available for the following controllers:- L20E
- L50E
- L70E
A data log supports up to 10 data sets and each data sets supports up to 128 variables. Use the
Data Log
configuration page to:- Add data sets to the controller configuration.
- Remove data sets from the controller configuration.
- Import data sets to or export data sets from an M8A file.
- Open the variable selector to add variables to a data set.
- Move a data set's variables up and down in the variable list.
Setting | Description |
|---|---|
Data set list | Lists the data sets in the project. The data set names are read-only. Select or clear the DEST<x> checkbox to add the data set to or delete the data set from the project. |
Import | Opens Import data log to import data sets from an M8A file. Import is available when the controller is offline. |
Export | Opens Export data log to export data sets to an M8A file. Export is available when the following conditions are met:
|
Data log details | Specifies the following information of the data set:
The dialog is available by selecting beside a selected data set. |
Manage data logs | Opens the <controller-name>: Manage data log page to do the following actions:
|
Provide Feedback
beside a selected data set.