Expansion modules
The 2085 expansion modules are attached to the right side of L50E and L70E controllers to extend their capabilities. The number of supported expansion modules varies with the controller type:
- L50E controllers with less than 24 digital I/O points support up to four expansion I/O modules and up to 132 digital I/O points.
- L50E controllers with 48 digital I/O points support up to four expansion I/O modules and up to 192 digital I/O points.
- L70E controllers support up to eight expansion I/O modules if a power supply module is attached, and support up to 304 digital I/O points.
In
FactoryTalk Design Workbench
, you can configure whether to fault the controller if an expansion module is absent. To check if an expansion module is present, use the MODULE_INFO instruction.The following image shows an L70E controller configuration with three expansion modules and a power supply module. The power supply module must be in slot 2, 3, 4, or 5.
Because the L70E expansion module does not have inputs or outputs, it uses a physical slot instead of a logical slot.
L70E controller with expansion modules

After adding an analog or digital expansion module to the controller:
- Global variables are created in the controller project to support the additional I/O points.
- The module's catalog and slot number are shown inProject Organizer. To open the expansion module's configuration page, inProject Organizer, go to , and then double-click the expansion module.
Model Number | Type | Description |
|---|---|---|
2085-IF4 | Multi-channel analog | 4-channel 14-bit analog and current input module |
2085-IF8 | Multi-channel analog | 8-channel 14-bit analog and current input module |
2085-IRT4 | Multi-channel analog | 4-channel RTD and TC temperature module |
2085-OF4 | Multi-channel analog | 4-channel 12-bit analog voltage and current output module |
2085-IA8 | Discrete I/O digital | 8-channel 120V AC input module |
2085-IM8 | Discrete I/O digital | 8-channel 240V AC input module |
2085-IQ16 | Discrete I/O digital | 16-channel 24V DC sink/source input module |
2085-IQ32T | Discrete I/O digital | 32-channel 24V DC sink/source input module |
2085-OA8 | Discrete I/O digital | 8-channel 120/240V AC output module |
2085-OB16 | Discrete I/O digital | 16-channel DC source output module |
2085-OV16 | Discrete I/O digital | 16-channel DC sink output module |
2085-OW16 | Discrete I/O digital | 16-channel relay output module |
2085-OW8 | Discrete I/O digital | 8-channel relay output module |
2085-EP24VDC | Power supply | 24V DC power supply module |
For more information about expansion modules, see Micro830, Micro850 and Micro870 Programmable Controller User Manual - 2080-UM002_-EN-E. | ||
Provide Feedback