Expansion module configuration page
After adding an expansion module to a controller, in
Project Organizer
, under Expansion
, a <expansion-module-catalog-number>
node is created.To open the expansion module configuration page, go to , and then double-click the expansion module.
On the expansion module configuration page, from the left pane, select a node to open the corresponding page.
Expansion Module | Pages Created |
|---|---|
Analog |
|
Digital |
|
Specialty | Overview |
For more information, see the introduction to individual expansion modules. | |
Provide Feedback