Add an expansion module to a controller project

Expansion I/O modules extend the capabilities of L50E and L70E controllers by optimizing the flexibility of the I/O count and type.
For L50E controllers:
  • Add no more than four expansion modules.
  • To avoid program compiling problems, limit the total number of digital inputs and outputs to:
    • 192 or less for L50E controllers with 48 digital I/O points.
    • 132 or less for other L50E controllers.
For L70E controllers:
  • Add no more than eight expansion modules and no more than one power supply expansion module.
  • To avoid program compiling problems, limit the total number of digital inputs and outputs to 304 or less.
To add an expansion module to a controller project
  1. In
    Project Organizer
    , go to
    I/O Configurations
    Expansion
    .
  2. Right-click
    Expansion
    , and then select
    New module
    .
  3. In
    Add module
    , select an expansion module, and then select
    Add
    .
  4. In
    Devices definition
    , select the slot, revision, and controller fault behavior as needed, and then select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal