Output pane
The
Output
contains the following pages that provide information about the project or the currently opened page in the workspace:- Log
- Error list
- Console
When opening the
Output
pane, the Log
page displays by default unless an error occurs, in which case the Error list
page is shown.Console page
Console page

Item | Name | Description |
|---|---|---|
![]() | Status overview pane | Lists the added devices. Select a device from the list to filter the log entries by device. When a device is selected, displays in the Device column, indicating that the column is filtered. |
![]() | Device | Lists the devices that are associated with the generated information. |
![]() | Description | Displays the logs about the added devices |
![]() | Time | Displays the time stamps of the logs. |
![]() | Search box | Enters the device name and log description to find and filter the logs. |
Error list page
Error list page

Item | Name | Description |
|---|---|---|
![]() | Scope list | Selects a scope to filter error messages by specific context or category. The scope is General by default. |
![]() | Search box | Enters the corresponding description, location, or device to find error messages that match. |
![]() | Errors button | Displays or hides the errors. |
![]() | Warnings button | Displays or hides the warnings. |
![]() | Messages button | Displays or hides the information messages. By default, errors, warnings, and messages are displayed on the Error list page. When there are errors, only errors are displayed. |
![]() | Description | Displays the message content. |
![]() | Location | Displays the location of errors and their links. |
![]() | Device | Displays the device name in which the error occurred. You can select in the column header to search or filter errors by device. |
Log page
Log page

Item | Name | Description |
|---|---|---|
![]() | Scope list | Selects a scope to filter log messages by specific context or category. The scope is General by default. |
![]() | Clear log button | Clears the log entries about the selected scope. |
![]() | Log entries | Displays the log entries in this controller project. |
Provide Feedback

displays in the 






in the column header to search or filter errors by device.