Pane bar
Use the pane bar to display or hide panes quickly. The following table introduces the button toggles on the pane bar.
Item | Name | Description | Keyboard Shortcut |
|---|---|---|---|
![]() | Left panes | Displays or hides the panes that are last pinned to the left side of the user interface (UI). | Ctrl+Shift+L |
![]() | Project Organizer | Displays or hides Project Organizer . | Ctrl+Shift+P |
![]() | Right panes | Displays or hides the panes that are last pinned to the right side of the UI. | Ctrl+Shift+R |
![]() | Toolbox | Displays or hides Toolbox . | Insert or Alt+Insert |
![]() | Properties | Displays or hides Properties . | Alt+Enter |
![]() | Connection | Displays or hides Connection . | Ctrl+Alt+C |
![]() | Bottom panes | Displays or hides the panes that are last pinned at the bottom of the UI. | Ctrl+Shift+B |
![]() | Output | Displays or hides Output . |
|
Provide Feedback