Search
FactoryTalk Design Workbench Help
Build a Traffic Light program
Perform the following tasks in
FactoryTalk Design Workbench
to create the Traffic Light project and controller program.
Tasks to create the Traffic Light project and controller program
No.
Task
1
Create a controller project
2
Add a plug-in module
3
Create a user-defined function block and variables
4
Add contacts to the first ladder rung
5
Add a time delay and two coils to the first ladder rung
6
Add a second ladder rung
7
Add additional rungs and edit variable assignments
8
Create a ladder diagram program
9
Add a user-defined function block to a ladder program
10
Assign input and output variables to the user-defined function block
11
Establish communications to the controller
12
Secure the controller with a password
13
Download the project to the controller
14
Test the running program
Getting-start project
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal