Add a plug-in module
Use the steps to enter a description for the controller and add two plug-in modules.
To add a plug-in module
- InProject Organizer, double-click the controller to open the controller workspace.
- Enter a description for the controller.
- From theControllertree, selectGeneral.
- On theGeneralconfiguration page, inDescription, enterTraffic Light.
- Add two plug-in modules to the controller.
- InProject Organizer, expandI/O Configurations.
- Right-clickPlug-in, and then selectNew module.
- InAdd module, select2080-MEMBAK-RTC2, and then selectAdd.
- InDevices definition, selectOK.
- Repeat steps from a through d to add the 2080-IF4 plug-in module to the controller.
- Save the project by doing one of the following:
- From the menu bar, select
. - From theFilemenu, selectSave.
Provide Feedback