Create a ladder diagram program
Use the steps to create a ladder diagram (LD) program, and then rename the program.
Prerequisites
To create a ladder diagram
- InProject Organizer, right-clickPrograms, and then selectNew program.
- InNew program, do the following:
- Enter the program nameTraffic_Light_Control.
- From theTypelist, selectLadder diagram.
- SelectCreate.
- Save the project by doing one of the following:
- From the menu bar, select
. - From theFilemenu, selectSave.
Provide Feedback