View ownership for an object
The Library Ownership window displays a list of all library object associations for the item highlighted in the
Selected Objects
column. The listing includes the object type and the library object or objects that the item is associated with. Items with multiple library object associations show multiple listings.
TIP:
When a selected object contains child objects, all of the child objects are included in the
Library Ownership
list.To view the ownership for a selected object
- Right-click the item in theSelected Objectscolumn and selectLibrary Ownership. TheLibrary Ownershipwindow opens.
- ClickNavigatefor a listing to open the owner library and display the decorator panel for the selected item.
Provide Feedback