Library Ownership window

The
Library Ownership
window shows the usage of an item by library objects. By default, items can be owned by multiple library objects, this is called shared ownership. If an item should be used exclusively by a single library object, disable shared ownership for the item.
This table describes the columns in the
Library Ownership
window.
Column
Description
Name
The name of the item.
Type
The type of the item.
Owner Library
The name of the library that contains the library object that references the item.
Navigate
Opens the owner library and displays the decorator panel for the selected item. Use this to learn the specific association for the listed item, where it is in the library object structure, and the context of its inclusion in the library object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal