Library Object Import Wizard

How do I open the Library Object Import Wizard?
  • In
    Logix Designer
    , right-click the ACD file object and select
    Plug-Ins > Import Library Objects
    .
Use the
Library Object Import Wizard
to connect to an ACM database and add library objects to the ACD file.
The Library Object Import Wizard includes:
  • Registered Libraries
    that display all libraries (classes) in the connected ACM database in a tree view. Select library objects to add them to the ACD file.
  • Content Configuration
    that display the properties and parameters of the selected objects. Edit the properties and parameters of the objects and link the objects to other objects or the ACD file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal