Add library objects to an ACD file
Use the Library Object Import Wizard to add library objects to an ACD file.
To add library objects to an ACD file
- InLogix Designer, right-click the ACD file object and selectPlug-Ins > Import Library Objects.
- In theLibrary Object Import Wizard, do one of the following:
- InRegistered Libraries, select one or more library objects. Drag the objects to theLibrary Object(s)column.
- InRegistered Libraries, double-click a library node.
- In theLibrary Object(s)column, right-click the blank cell and selectAdd New.
- Configure the parameters of every object and clickNext.TIP:
- When adding one object, all parameters are shown in theACD Tag Browser.
- When adding two or more objects, link the current library objects to other library objects with one of the following methods:
- InIO Configuration, selectLink to Existing instanceto link to other library objects added to theLibrary Object(s)column.
- InIO Configuration, selectLink to an ACD instanceto link to the existing controller or program tags. Choose a tag in theACD Tag Browserdialog box.
- Click theOverride Calculated Parametersbutton to unlock the calculated parameters.
- (optional) Configure values of unresolved parameters and clickNext.TIP:
- Double-click the unresolved parameter to open the Edit Unresolved Name Substitution dialog box.
- In some cases such as a conditional expression, the unresolved parameter value may be part of the substitution to simplify resolving the value. Double-click in the Text field in the occurrences section that will automatically populate the value field for further editing.
- (optional) Merge the new content with the existing content and clickNext.
- Configure the content preview and clickNext.
- (optional) Check the import log file if the import process fails. Close theLibrary Object Import Wizardand open the ACD file to discard the failed changes.
Provide Feedback