Currency
The currency dashboard allows user to configure relevant currencies and set conversion factors directly from the global currency dashboard. It displays the exchange rates from the Site to the Region level and from the Site to the enterprise level. The system uses static and customizable exchange rates to convert costs between currencies.
- From the left panel, clickSettings.
- Under theConfigurationdropdown and clickCurrencies. The Currency dashboard is displayed.Currencies

Provide Feedback