Use FactoryTalk Diagnostics Counter Monitor with FactoryTalk Linx Gateway
FactoryTalk Diagnostics Counter Monitor
aids in troubleshooting OPC connections from third-party products. It shows diagnostic information about the FactoryTalk Linx Gateway
runtime operation:
TIP:
To prevent
FactoryTalk Linx Gateway
performance degradation, run only one instance of FactoryTalk Diagnostics Counter Monitor
at a time, and close the tool when you have finished troubleshooting.- Diagnostics counters are shown as properties at various levels for theFactoryTalk Linx GatewayDA server,FactoryTalk Linx GatewayOPC UA server,FactoryTalk Linx GatewayDDE server,FactoryTalk Linx GatewayRTD server, andFactoryTalk Linx GatewayMQTT server.
- Individual diagnostic items are shown as children of their corresponding group connections.

Provide Feedback