FactoryTalk Linx Gateway DDE diagnostics values
The following internal diagnostic values, counters and strings are made available by FactoryTalk Linx Gateway DDE server for diagnostic purposes. These diagnostic values track activity at the boundary between the DDE client and FactoryTalk Linx Gateway DDE server, and they are supported by FactoryTalk Diagnostics Counter Monitor.
The diagnostic counters display cumulative values since the FactoryTalk Linx Gateway DDE service initially starts. The counters are reset only when the service is stopped and restarted.
Name | Type |
|---|---|
LicenseName | Value |
LicenseCount | Counter |
Count against Activation | Counter |
Service Status | Value |
Client Connect calls | Counter |
Client Disconnect calls | Counter |
Client Call OnRequest | Counter |
Client Call OnPoke | Counter |
Client Call OnAdvStart | Counter |
Client Call OnAdvStop | Counter |
Provide Feedback