Set the default options

Use the
Settings
dialog box to set default options for the
Solutions
,
Library Types
,
Categories
, and
Families
items in the
Properties
panel.
To set the default options for library object classification
  1. Click
    SETTINGS > Library Attributes
    .
    The Settings dialog box opens displaying the
    Solutions
    ,
    Library Types
    ,
    Categories
    , and
    Families
    items.
    A button with an ellipsis (...) follows each item.
  2. To define the default options for an item, click the corresponding ellipsis button.
  3. The
    List Editor
    dialog box opens. Enter the options for the items, one per line.
  4. Click
    OK
    to accept the options and return to the
    Settings
    dialog box. Repeat for all of the items as needed.
  5. Click
    OK
    to save the changes and close the
    Settings
    dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal