Settings dialog box reference

Use the
Settings
dialog box to set default options for the
Solutions
,
Library Types
,
Categories
, and
Families
items in the
Properties
panel.
This table describes the items in the
Settings
dialog box. To configure an item or create a list of items, click the corresponding ellipsis (...) button.
Item
Description
Solutions
The library object repository for a set of library objects.
Library Types
The general classification for a library object based on its function. For example, module, value, or motor.
Categories
A more specific classification for a library object, based on its function. For example, digital, analog, communication, or controller type.
Families
The specific identifier for the base catalog number of the item. For example, 1734, 1738, Logix, or Project.
Default the Publish Status to Pending
Select to set pending as a default library status.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal