Expression Builder
How do I open Expression Builder?
- InLibrary DesignerorLibrary Object Manager, select the ellipsis button (...) next to parameters, values, and other objects that can be modified by or decorated with an expression.
The
Expression Builder
is an environment to create, test, and save expressions.
The
Expression Builder
window includes a command toolbar, decorative element tabs, and functional areas.Item | Description |
|---|---|
![]() | The Add New button is only active on the Parameter tab and opens the Add New Parameter window. |
![]() | The Move Up/Move Down buttons are not active in the Expression Builder window. |
![]() | This dropdown menu can initiate a search for parameters that match a text string entered in the adjacent field. There are two different types of finds that can be performed, use the dropdown menu to select the one to use:
Find can be used on all of the tabs. |
The decorative elements available to the current expression. These include all elements added to the current library object and all elements added to the library objects that are higher in scope. These elements include:
Functions and expressions can be saved and used in future projects. | |
A collection of logical and mathematical operators that can be used to manipulate the values generated by the decorative elements. | |
Expression box and Result Type | The expression appears here as elements are added to it. There are also settings and buttons to set the data type of the expression result, and to validate, test, and save the expression. The Result Type displays a color-coded response when the expression is validated and tested. |
Provide Feedback