Decorative elements tabs

The decorative elements tabs display the properties available to the current expression. These include all elements added to the current library object and all elements added to the library objects that are higher in scope. Tabs are used to organize the different actions that can be taken on each element:
  • Parameters
    Use this tab to add new parameters to the expression, edit the existing parameters, delete a parameter from the expression, copy an existing parameter, show references to other uses of the parameter, and move the parameter up or down in the instantiation order of the expression.
  • Functions
    Use this tab to add new functions to the expression, edit the existing functions, delete a function from the expression, copy an existing function, paste an existing function, and show references to other uses of the function.
  • Expressions
    Use this tab to add an existing expression to the selected library object. Using saved expressions eliminates repetitive expression coding when multiple fields use the same expression, or when an existing expression can be used as a template. Double-click an expression from either the
    Most Recently Used
    or
    Saved
    lists to add that expression to the Expression box. If needed, expressions can be deleted from the expressions list using this tab. The
    Library Designer
    saves a running list of the last ten expressions created in the
    Expression Builder
    . Saved expressions are available to all projects opened in the
    Library Designer
    .
    Both functions and expressions can be saved within the
    Library Designer
    and used in future projects.
  • Predefined
    Use this tab to add items from the list of global and local parameters that are available to all library objects to the expression. Predefined parameters cannot be modified, deleted, copied, or pasted.
    IMPORTANT:
    Saved and recently used expressions are carried over from previous projects.
    The decorative elements in these expressions may not be present in the current project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal