Create an audit trail detail object
You may need to create an audit trail detail object to view the details of an audit entry on a graphic display.
To create an audit trail detail object
- In theGraphics Displayeditor, selectObjects > Advanced > Audit > Audit Trail Detailor drag
from the toolbox. - Drag the mouse to draw a rectangle of the general size and in the general location you want the button to be.
- Double-click the button to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how the object looks.
Provide Feedback