Audit trail detail object
    Audit trail detail object shows the information about the selected audit entry on an audit trail list, including:
- Occurred time- The local date and time when the software product records the action as having occurred.
- Source- The name of the software product that logged the action in the audit log.
- Location- The name of the computer, Windows CE device, orMobileViewterminal on which the action took place.
- Resource-Reserved
- Username- The login ID of the user who is using the software product. This can be aFactoryTalk Securityuser or aMicrosoftWindowsuser, depending on how the user logged into the software product that generated the audit record.
- Message- Information about a specific operator action executed within the context of the running runtime application. For example, the message for a tag write will include the tag being modified, and the tag’s previous and new values.
Clear Audit Trail
 button and the following Key 
buttons to interact with an audit trail detail object:- Move up
- Move down
Provide Feedback