Options on the Audit tab of the Audit Trail Detail Properties dialog box
The following table shows the options on the
Audit
tab of the Audit Trail Detail Properties
dialog box.Options | Descriptions |
|---|---|
Rows | Specify which rows to use, their time and date format, and what header text they will show, if any. |
Select a row | Select a row to be edited:
|
Display row | Select this check box if you want the selected row to appear in the object. |
Time and date format | Select the time and date format to show. The available options reflect the settings in your development computer’s operating system. In Windows, these are found in the Regional and Language options in the Control Panel . If the operating system settings are different on your development and runtime systems, the runtime settings are used at runtime.This option is available only when Occurred Time is selected. |
Header text | Type the text to show for the header of the selected row. |
Word wrap | Select this check box if you want the text to continue on the next line at the beginning of a new word. If this check box is cleared, the text continues on the next line whenever the maximum text length is reached, even if this occurs in the middle of a word or number. The maximum text length depends on the width of the object and the font size. |
Provide Feedback