Validation Errors
The Studio 5000 Logix Designer application performs a validation check when you change the
connection type or channel modes in the Device Definition and select OK.
If the change is not allowed, an error message appears.
Provide Feedback