Channel xx Mode from Fallback to IO-Link

When an IO-Link device exists on the channel and you change the channel mode from "Digital Input, Fallback" or "Digital Input, Timestamp, Fallback" to "IO-Link", consider the following:
  • The IO-Link device that is on the channel uses the default process data definition.
  • Any changes that are pending in the IO-Link Device Properties are lost.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal