Channel xx Mode from IO-Link to Fallback
When an IO-Link device exists on the channel and you change the channel mode from "IO-Link" to "Digital Input, Fallback" or "Digital Input, Timestamp, Fallback", consider the following:
- The channel mode change fails if the IO-Link device that is on the channel does not support the standard input/output mode.
- The IO-Link device that is on the channel uses the Heartbeat connection.
- Any changes that are pending in the IO-Link Device Properties are lost.
Provide Feedback