- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
IUANode.GetVariable(browsePath)
Returns an
IUAVariable
C# object. The returned object corresponds to the first child variable of the node on which the method is invoked. The returned object name corresponds to the argument.IUAVariable GetVariable(stringbrowsePath);
Arguments
- browsePath(string)
- Can be either:
- TheBrowseNameof the object
- The path of the object in the information model, uniquely expressed as a sequence ofBrowseNamevalues separated by/
Returns
- IUAVariable
- A C# Object that matches the requested variable.
Examples
The following examples show a returned C# object that corresponds to the
Speed
variable of the Motor1
object:
var currentSpeed = Project.Current.GetObject("Motor1").GetVariable("Speed")
var currentSpeed = Project.Current.GetVariable("Motor1/Speed");
Provide Feedback