Motion Move Instructions

Use the Motion Move instructions to control axis position.
Available Instructions
Ladder Diagram and Structured Text
Function Block
Not available
IMPORTANT: Tags used for the motion control attribute of instructions should only be used once. Re-use of the motion control tag in other instructions can cause unintended operation. This may result in damage to equipment or personal injury.
The Motion Move instructions are:
If you want to:
Use this instruction:
Stop any motion process on an axis.
MAS
Home an axis.
MAH
Jog an axis.
MAJ
Move an axis to a specific position.
MAM
Start electronic gearing between two axes.
MAG
Change the speed, acceleration, or deceleration of a move or a jog that is in progress.
MCD
Change the command or actual position of an axis.
MRP
Calculate a Cam Profile based on an array of cam points.
MCCP
Calculate the slave value, slope, and derivative of the slope for a cam profile and master value.
MCSV
Start electronic camming between two axes.
MAPC
Start electronic camming as a function of time.
MATC
Define a Master/Slave relationship between two motion axes and select which type of move instructions.
MDAC
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal