Master Driven Axis Control (MDAC)

This information applies to the
CompactLogix
5370,
ControlLogix
5570,
Compact GuardLogix
5370,
GuardLogix
5570,
Compact GuardLogix
5380,
CompactLogix
5380,
ControlLogix
5580,
GuardLogix
5580, and ControlLogix 5590 controllers.
The Master Driven Speed Control (MDSC) function provides the ability to synchronize one or more motion axes to a common Master Axis. The MDSC uses the Master Driven Axis Control (MDAC) instruction, which assigns a Master:Slave relationship for single axes.
Using the MDSC function provides synchronization of axes without the use of CAM profiles. The MDSC functions may also be used with Time Driven CAM profiles (MATC) to make them act like position driven profiles synchronized with a Master Axis.
This is a transitional instruction. Follow these steps when using it:
  • In ladder logic, insert an instruction to toggle the rung-condition-in from false to true each time the instruction should execute.
  • In a Structured Text routine, insert a condition for the instruction to cause it to execute only on a transition.
Available Languages
Ladder Diagram
Function Block
This instruction is not available in function block.
Structured Text
MDAC (SlaveAxis, MasterAxis, MotionControl, MotionType, MasterReference);
Operands
Ladder Diagram
Operand
Type
TIP: AXIS_CONSUMED is supported by
Compact GuardLogix
5580, and
CompactLogix
5380 controllers only.
Type
TIP: AXIS_GENERIC is supported by the
ControlLogix
5570 and the
GuardLogix
5570 controllers only.
Format
Description
Slave Axis
AXIS_CIP_DRIVE
AXIS_VIRTUAL
AXIS_SERVO
AXIS_SERVO_DRIVE
AXIS_GENERIC_DRIVE
AXIS_CIP_DRIVE
AXIS_VIRTUALAX
Tag
The Single Axis being controlled by the Master Axis when the motion planner is in Master Driven mode. Ellipsis launches Axis properties dialog.
The MDAC link is broken when the following instructions are executed:
On the Slave Axis: MAS (All), MCS (All), MGS, MASD, MCSD, MGSD, a mode change. Note that MAS (anything other than All) and MCS (coordinated) do NOT break the MDAC link.
The Shutdown instructions (MGSD, MASD, MCSD) never go IP.
On the Master Axis: MASD, MCSD, and MGSD. Note that MAS and MCS for any Stop Type, including All, do NOT break the MDAC link.
A mode change (Rem Run to Rem Prog or Rem Prog to Rem Run) or an axis fault also breaks the MDAC link.
Master Axis
AXIS_CONSUMED
AXIS_CIP_DRIVE
AXIS_VIRTUAL
TIP: AXIS_CONSUMED is supported by
Compact GuardLogix
5580, and
CompactLogix
5380 controllers only.
AXIS_CONSUMED
AXIS_SERVO
AXIS_SERVO_DRIVE
AXIS_GENERIC_DRIVE
AXIS_CIP_DRIVE
AXIS_VIRTUAL
Tag
Any configured Single Axis that the Slave Axis follows. The Master Axis can be any axis that has been configured.
Ellipsis launches Axis properties dialog.
Motion Control
MOTION_INSTRUCTION
MOTION_INSTRUCTION
Tag
Control tag for the instruction.
Motion Type
UNIT32
UNIT32
Immediate or Tag
Specifies the move type (MAM, MAJ, MATC, or MAM - Master Offset Move for a Position Cam) executing on the Slave Axis that will be controlled by the Master Axis when a single axis motion instruction is programmed in Master Driven Mode. The enumerations for Motion Type are:
All = 0
Move = 1
Jog = 2
Time Cam = 3
Master Offset Move = 4
Master Reference
UNIT32
UNIT32
Immediate or Tag
Selects the Master Axis position source as either Actual Position (0) or Command Position (1).
The All for the motion type lets the system know that Master Driven Mode applies to all single axis instructions (that is, MAM, MAJ, MATC, and a MAM (Master Offset Move)). If the Motion Type of the active MDAC is set to anything other than All on a Slave Axis, then executing a MDAC All on the Slave Axis causes a runtime error. For example:
MDAC Move=MAM Master=X Slave=Y - Assigns master and slave axes
MDAC Move=ALL Master=Z Slave=Y - Causes an error because the previous MDAC assigned the MAM to the Y axis. Note that assigning the Slave Y axis to any other Master axis causes the same error because Y is already assigned to a MAM.
To be able to reassign the Master once the All option is used, it is sufficient to execute one of the following for either the Slave Axis or the Master Axis, although you can also choose to execute one of the following for both the Slave Axis and the Master Axis:
  • On the Slave Axis: MAS (All), MCS (All), MGS, MASD, MCSD, or MGSD
  • On the Master Axis: MASD, MCSD, or MGSD
If there is an active MDAC (All) on a Slave, then setting the MDAC instruction to a Motion Type other than All causes a runtime error.
To be able to reassign the Master once anything other than the All option is used, you must execute any of the following:
  • on the Slave Axis: MAS (All), MCS (All), MGS, MASD, MCSD, or MGSD
  • On the Master Axis: MASD, MCSD, or MGSD
If you assign the same axis to be both a Master and a Slave Axis, an
RSLogix
5000 software verification error is generated.
The same Slave axis can be assigned to 2 different Master axes. For example, if X, Y are the Master axes and Z is a Slave axis, then X can be assigned to be the Master axis for MAM instructions for Z and Y is the Master axis for MAJ instructions for Slave Z. Refer to the following illustration.
MDAC_master_slave axes diagram.png
The Master Axis for an active Slave may be changed by executing a MDAC for the slave with a different Master. The MDAC puts the pending Master in a queue for the Slave. When the next single axis motion instruction is executed (goes IP) in either Replacement or Merge mode, the queued Master Axis becomes the Master for the Slave the next time a single axis motion is started. For example:
In this example, the masters are already running.
MDAC Move=MAM Master=X Slave=Z
Assigns master and slave axis
MAM X
Start MAM motion on the master 1
MAM Z
Start MAM motion on the slave
MAM Y
Start MAM motion on the Y master 2
MDAC Move=MAM Master=Y Slave=Z
Y is pending to be the new master
MAM Z
Start new MAM motion on the slave using new master 2
Use different control words on all MDAC instructions. If the same control word is used for the active and pending MDAC, the IP bit of the pending MDAC will not work properly. When separate axis control words are used for the active and the pending MDAC instructions, the active and the pending MDAC will both have their IP bits set. However, only the active MDAC will have its AC bit set. This is standard operation for all instructions. No detection of the same control word used on multiple instructions is made.
Master Reference
The Master Reference for an MDAC instruction selects the Master Axis position source.
The enumerations for Master Reference Axis are:
Actual – Slave motion is generated from the actual (current) position of the Master Axis as measured by its encoder or other feedback device.
Command – Slave motion is generated from the command (desired) position of the Master Axis.
Because there is no Command Position for a Feedback Only Axis, if you select either Actual or Command for Master Reference, the Actual Position of the Master Axis is used. The Actual and Command Position are always the same for this case. No error is generated.
Because there is no Actual Position for a Virtual axis, if you select either Actual or Command for Master Reference, the Command Position is used. No error will be generated.
An error is generated if a MDAC instruction is executed that changes the Master Reference of a slave axis that is in motion. The new MDAC instruction will error and the original one will remain active.
Structured Text
Operand
Type
Format
Description
Source
SINT
INT
DINT
REAL
STRING
structure
tag
Initial element to copy
IMPORTANT: The Source and Destination operands should be the same data type, or unexpected results may occur
Destination
SINT
INT
DINT
REAL
STRING
LINT
structure
tag
Initial element to be overwritten by the Source
IMPORTANT: The Source and Destination operands should be the same data type, or unexpected results may occur
Length
DINT
immediate or tag
Number of Destination elements to copy
See Structured Text Syntax for more information on the syntax of expressions within structured text.
Note that you have the option to browse for enumerations in the Structured Text Editor as shown in the following.
MDAC_Other_Pg482_v31
MOTION_INSTRUCTION Bit Leg Definitions for MDAC
Mnemonic
Description
.EN (Enable) Bit 31
The enable bit is set when the rung transitions from false-to-true and stays set until the rung goes false.
.DN (Done) Bit 29
The done bit is set when the Master Driven Axis Control instruction is successfully initiated.
.ER (Error) Bit 28
The error bit is set when there is an invalid combination of parameters in the MDAC instruction.
.IP (In Process) Bit 26
The in process bit is set when the MDAC instruction is activated and reset by an instruction (for example, the MASD instruction).
.AC (Active) Bit 23
The active bit is set when a move (MAJ, MAM or MATC) goes IP in Master Driven mode on the axis that is selected as the Slave Axis of the MDAC instruction. If the Slave Axis is started in Time Driven mode, then the AC bit of the MDAC does not go active. The IP bit of the MDAC instruction does not change at this time.
Description
The MDAC instruction is used to select a single axis as a Master Axis and a single axis as a Slave Axis. The MDAC instruction connects a Master and Slave Axis for a MAM, MAJ, and MATC instruction. When an MDAC is executed (goes IP), the specified Slave Axis in the MDAC instruction is logically geared with the designated Master Axis. After motion on both the Master and Slave Axes has been initiated, the Slave follows the Master Axis motion using the programmed dynamics of the motion instruction.
There are no changes in any active motion when a new MDAC instruction is activated. Activating a new MDAC instruction puts the parameters programmed in the MDAC into a pending state. The parameters in the pending MDAC instruction are overridden if you execute a succeeding MDAC before a new single axis motion instruction (MAM, MAJ, and MATC) is activated on the slave axis. The most recent values in the pending MDAC instruction are used when a new single axis motion instruction is activated on the Slave Axis.
A MATC with an Execution Schedule of Pending always uses the Instruction mode of the active MATC; Lock Position and Lock Direction are ignored. This is explained further in the following example.
Assume that there are four instructions executed in the following order:
  • MDAC1: Master=X, Slave=Y
  • MATC1: Slave Y, Immediate
  • MDAC2: Master=Z Slave=Y MDAC2 is executed (goes IP) while MATC1 is moving (Master Axis is changed)
  • MATC2: Slave=Y, Pending
  • MATC2: will use the parameters from MDAC1 (Master and Slave) because MATC1 was moving (active) when MDAC2 was executed. If MATC2 and MDAC2 were executed in the reverse order, you get the same results. This follows the existing paradigm of MAPC instruction where the pending CAM uses the same master as the running CAM.
Motion Direct Command and the MDAC Instruction
To obtain Motion Direct support for Master Driven Speed Control mode, you must first program an MDAC in one of the supporting program languages before you execute an MAM or MAJ in Time driven Mode.
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See the Common Attributes for operand-related faults.
Execution
Ladder Diagram
Condition/State
Action Taken
Prescan
The .EN, .DN, .ER, and .IP bits are cleared to false.
Rung-condition-in is false
The .EN bit is cleared to false if either the .DN or .ER bit is true.
Rung-condition-in is true
The .EN bit is set to true and the instruction executes.
Postscan
N/A
Structured Text
Condition/State
Action Taken
Prescan
See Prescan in the Ladder Diagram table.
Normal execution
See Rung-condition-in is false in the Ladder Diagram table.
Postscan
See Postscan in the Ladder Diagram table.
Error Codes
See Motion Error Codes .ERR for run time errors for motion instructions when MDAC is active.
Verification Errors
An invalid or No Master Axis will cause new errors to be generated when verified by the programming software. The following conditions may cause this error:
  • The Master and Slave Axis are the same.
  • Master or Slave Axis is not configured.
  • Master or Slave Axis is inhibited.
  • Redefine position is in progress.
  • Home of an axis is in progress.
MDSC ALL Conflict. The ALL parameter is not allowed while a Slave axis motion generator (for example, the jog motion generator) is already assigned.
Examples
Example 1
Ladder Diagram
MDAC_LD_ex1_v31
Example 2
Ladder Diagram
MDAC_LD_ex2_v31
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal