Motion Axis Stop (MAS)
This information applies to the
CompactLogix
5370, ControlLogix
5570, Compact GuardLogix
5370, GuardLogix
5570, Compact GuardLogix
5380, CompactLogix
5380, ControlLogix
5580, GuardLogix
5580, and ControlLogix 5590 controllers.Use the Motion Axis Stop (MAS) instruction to stop a specific motion process on an axis or to stop the axis completely.
Architecture | Standard | Safety |
---|---|---|
CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, and GuardLogix
5570 controllers | Yes | No |
CompactLogix 5380, ControlLogix 5580, Compact GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers | Yes | No |
Available Languages
Ladder Diagram

Function Block
This instruction is not available for function block.
Structured Text
MAS(Axis,MotionControl,StopType,ChangeDecel,DecelRate,DecelUnits,ChangeDecelJerk,DecelJerk,Jerk Units)
Operands
Ladder Diagram
Operand | Type
TIP:
AXIS_CONSUMED is supported by
Compact
GuardLogix 5580, and CompactLogix 5380 controllers only. | Type
TIP:
AXIS_GENERIC is supported by the
ControlLogix 5570 and the GuardLogix 5570 controllers
only. | Format | Description | |
---|---|---|---|---|---|
Axis | AXIS_CIP_DRIVE AXIS_VIRTUAL | AXIS_CIP_DRIVE
AXIS_VIRTUAL
AXIS_GENERIC
AXIS_GENERIC_DRIVE
AXIS_SERVO
AXIS_SERVO_DRIVE ControlLogix 5570, GuardLogix 5570, ControlLogix
5580, GuardLogix 5580, and ControlLogix 5590
controllers | Tag | Name of the axis. For controllers that support the REF_TO motion data types, the
supported axis operand type can be replaced by an equivalent REF_TO type. | |
Motion Control | MOTION_INSTRUCTION | Tag | Control tag for the instruction. | ||
Stop Type | DINT | Immediate | To Stop | Choose this Stop Type | |
All motion in process for this axis. | All = 0 With this selection, the instruction stops all motion on an axis. The stops takes any coordinated motion on the axis into account when it computes the Decel rate and stops that component of the coordinated motion. The other axes components of the coordinated motion are unaffected and continue. If this instruction stops a Motion Drive Start (MDS) instruction, the Direct Control Feature is disabled and the affected axis is decelerated to a stop using the instruction parameters. | ||||
Only a certain type of motion but leave other motion processes running. | Choose the type of motion that you want to stop: | ||||
Jog = 1 | |||||
Move = 2 | |||||
Gear = 3 | |||||
Home = 4 | |||||
Tune = 5 | |||||
Test = 6 | |||||
Time Cam = 7 | |||||
Position Cam = 8 | |||||
Master Offset Move = 9 | |||||
Direct Control = 10 (1) | |||||
The axis could still be moving when the MAS instruction is complete. | |||||
Change Decel | DINT | Immediate | If you want to | Then Choose | |
Use the Maximum Deceleration rate of the axis. | No = 0 | ||||
Specify the deceleration rate. | Yes = 1 | ||||
Decel Rate | REAL | Immediate or Tag |
IMPORTANT:
The axis could overshoot its target
position if you reduce the deceleration while a move is in process.
Deceleration rate of the axis. The instruction uses this value only if Change Decel is Yes. | ||
Decel Units | DINT | Immediate | Which units do you want to use for the Decel Rate?
| ||
Change Decel Jerk | DINT | Immediate | If you want to | Then Choose | |
Use the Maximum Deceleration Jerk rate of the axis. | No (0) | ||||
Program the deceleration jerk rate. | Yes (1) | ||||
Decel Jerk | REAL | Immediate or Tag |
IMPORTANT:
The axis could overshoot its target
position if you reduce the deceleration jerk while a move is in process.
You must always enter a value for the Decel Jerk operand. This instruction only uses the value if the Profile is configured as S-curve.Decel Jerk is the deceleration jerk rate of the axis. Use these values to get started. Decel Jerk = 100 (% of Time) 0 = Units per sec 3 1 = % of Maximum 2 = % of Time (use this value to get started) | ||
Jerk Units | DINT | Immediate |
(1)
When the MAS instruction is used to with either an All or DirectVelocityControlStatus Command Stop Type, the selection also clears the MDS In Process (.IP) bit, and clears the Axis DirectVelocityControlStatus bit in the Motion Status attributeStructured Text
This Operand | Has These Options Which You | |
---|---|---|
Enter as Text | Or Enter as a Number | |
Stop Type | all jog move gear home tune test timecam positioncam masteroffsetmove directcontrol | 0 1 2 3 4 5 6 7 8 9 10 |
Change Decel | no yes | 0 1 |
Decel Units | Units per sec 2 %ofmaximum | 0 1 |
Change Decel Jerk | no yes | 0 1 |
Decel Jerk | no enumeration | You must always enter a value for the Decel Jerk operand. This instruction only uses the value if the Profile is configured as S-curve.Decel Jerk is the deceleration jerk rate of the axis. Use this value to get started. Decel Jerk = 100 % of Time (2) |
Jerk Units | unitspersec 3 % of Maximum % of Time | 0 1 2 |
See Structured Text Syntax for
more information on the syntax of expressions within structured text.
MOTION_INSTRUCTION Structure
To See If | Check To See If This Bit Is Set To | Data Type | Notes |
---|---|---|---|
A false-to-true transition caused the instruction to execute. | EN | BOOL | The EN bit stays set until the process is complete and the rung goes false. |
The stop was successfully initiated. | DN | BOOL | |
An error happened. | ER | BOOL | |
The axis is stopping. | IP | BOOL | Any of these actions end the MAS instruction and clear the IP bit:
|
The axis is stopped. | PC | BOOL | The PC bit stays set until the rung makes a false-to-true transition. |
Description
Use the MAS instruction when you want a decelerated stop for any controlled motion in process for the axis. The instruction stops the motion without disabling the servo loop. A trapezoidal profile is always used for MAS with Stop Type=ALL for the deceleration regardless of the programmed profile type. Use the instruction to:
- stop a specific motion process such as jogging, moving, or gearing
- stop the axis completely
- abort a test or tune process initiated by a Motion Run Hookup Diagnostics (MRHD) instruction or Motion Run Axis Tuning (MRAT) instruction.If the Stop Type isThen the MAS Instruction Uses This ProfileJogSame type of profile as the Motion Axis Jog (MAJ) instruction that started the jog.MoveSame type of profile as the Motion Axis Move (MAM) instruction that started the move.None of the aboveTrapezoidal.
When MAS ( Stop Type = All ) is used on any axis associated with a coordinate system and a coordinated motion instruction is running on it, Coordinate system’s maximum deceleration is used to stop remaining axes. If the coordinate system contains orientation axes, Coordinate system’s Orientation maximum deceleration is used for stopping remaining Rx, Ry or Rz axes.
Example
Suppose you use a Motion Axis Jog (MAJ) instruction with an S-curve profile to start a jog. Then you use an MAS instruction with a Stop Type of Jog to stop the jog. In that case, the MAS instruction uses an S-curve profile to stop the jog.
Programming Guidelines
WARNING:
Risk of Velocity and/or End Position Overshoot
If you change move
parameters dynamically by any method, that is by changing move dynamics [Motion Change
Dynamics (MCD) instruction or Motion Coordinated Change Dynamics (MCCD)] or by starting a
new instruction before the last one has completed, be aware of the risk of velocity and/or
end position overshoot.
A Trapezoidal velocity profile can overshoot if maximum
deceleration is decreased while the move is decelerating or is close to the deceleration
point.
An S-curve velocity profile can overshoot if:
- Maximum deceleration is decreased while the move is decelerating or close to the deceleration point; or
- Maximum acceleration jerk is decreased and the axis is accelerating. Keep in mind, however, that jerk can be changed indirectly if it is specified in % of time.
For more information, see Troubleshooting Axis Motion.
Guidelines | Details | |
---|---|---|
In ladder diagram, toggle the rung condition each time you want to execute the instruction. | This is a transitional instruction:
| |
In structured text, condition the instruction so that it only executes on a transition. | In structured text, instructions execute each time they are scanned.
For more information, see Structured Text Syntax. | |
Choose whether to stop all motion or only a specific type of motion. | If You Want to Stop | Then Choose This Stop Type |
All motion in process for this axis. | All The instruction uses a trapezoidal profile and stops the axis. | |
Stop only a certain type of motion but leave other motion processes running. | The type of motion that you want to stop The axis could still be moving when the MAS instruction is complete. The instruction uses an S-curve profile to stop the axis only if:
| |
Example: Suppose your axis is executing both a jog and a move at the same time. And suppose you want to stop only the jog but leave the move running. In that case, choose a Stop Type of Jog. | ||
To stop gearing or camming, select the slave axis. | To stop a gearing or position camming process, enter the slave axis to turn off the specific process and stop the axis. If the master axis is a servo axis, you can stop the master axis which in turn stops the slave without disabling the gearing or position camming.
TIP:
If the Master axis is moved manually while
the Master axis was in a disabled state, the actual position of the slave axis
continues to track the Master's position, regardless whether the
MasterReference of the MAPC instruction is set to Actual or Command.
| |
To stop a Master Offset move, enter the slave axis but use master units. | To stop an Absolute or Incremental Master Offset move:
| |
Be careful if the instruction changes motion parameters. | When you execute an MAS instruction, the axis uses the new deceleration and jerk rates for the motion that’s already in process. This can cause an axis to overshoot its speed, overshoot its end position, or reverse direction. S-curve profiles are more sensitive to parameter changes. For more information, see Troubleshoot Axis Motion . | |
Use the jerk operands for S-curve profiles. | Use the jerk operands when
Under those conditions, the instruction uses an S-curve profile to stop the axis. The instruction uses a constant deceleration rate for all other types of stops. You must fill in the jerk operands regardless of the type of stop. | |
Use % of Time for the easiest programming and tuning of jerk. | For an easy way to program and tune jerk, enter it as a % of the acceleration or deceleration time. For more information, see Tune an S-curve Profile . |
Master Driven Speed Control (MDSC) and the MAS Instruction
If the MAS is executed (goes IP) on the Slave Axis in Master Driven Mode, the MDSC link is immediately broken. The Slave always stops in Time Driven Mode, regardless if the active mode is Time Driven or Master Driven.
Stop Type for MAS
The behavior of the MAS instruction depends on the Stop Type parameter:
- Time CAM, stop type moves, and jogs - When you invoke an MAS with Stop Type = Time Cam on an axis that is running in Master Driven Mode, the axis terminates Master Driven Mode, changes to Time Driven Mode, and stops as specified.
- Master Offset Move - When you invoke an MAS with Stop Type = Master Offset Move on an axis that is running in Master Driven Mode and controlling a Position Cam, the offset axis terminates Master Driven Mode, changes to Time Driven Mode, and stops at the specified deceleration and deceleration jerk.
- All - When you invoke an MAS with Stop Type = All, the MDSC link is broken immediately. All motion planners on the specified axis terminate Master Driven Mode and axes are stopped at the specified deceleration and deceleration jerk in Time Driven Mode.
If the axes are involved in any coordinated motion (in Master Driven Mode), then the axes break from the coordinate motion planner and the other axes in the coordinate system continue. The IP bit is cleared on the Master Driven Axis Control (MDAC).
Note that MAS ALL on the Master axis does not break the MDSC link. For all other stop types in which you execute an MAS instruction on an axis that is being controlled in Master Driven Mode, the motion planner terminates Master Driven Mode on the requested axis for the requested Stop Type, changes to Time Driven Mode, and stops at the specified deceleration and deceleration jerk in Time Driven Mode. Other stop types do not clear the IP bit on the MDAC.
The AC bit of the MDAC instruction resets when the axis is stopped.
MAS All reset the IP bit of the MDAC. Other stop types do not reset the IP bit.
Note that if a stop is issued very close to the programmed endpoint, the actual stop may be beyond the programmed endpoint, especially if run in Master Driven Mode.
The status bit CalculatedDataAvailable in an active motion instruction status word for an MAS instruction resets when an MAS is executed (goes IP). The CalculatedData is not recomputed.
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. A major fault can occur if an uninitialized reference or
a reference of incorrect type is passed to the Axis Operand. See Common Attributes for operand related faults.
Execution
Ladder Diagram
Condition/State | Action Taken |
---|---|
Prescan | The .EN, .DN, .ER, and .IP bits are cleared to false. |
Rung-condition-in is false | The .EN bit is cleared to false if the .DN or .ER bit is true. |
Rung-condition-in is true | The .EN bit is set to true and the instruction executes. |
Postscan | N/A |
Structured Text
Condition/State | Action Taken |
---|---|
Prescan | See Prescan in Ladder Diagram table |
Normal execution | See Rung-condition-in is false, followed by rung is true in the Ladder Diagram table. |
Postscan | See Postscan in Ladder Diagram table. |
Error Codes
Extended Error Codes
Use Extended Error Codes (.EXERR) for more instructions about an error. See Motion Error Codes .ERR.
If ERR is | And EXERR is | Then | ||
---|---|---|---|---|
Cause | Corrective Action | |||
13 | Varies | An operand is outside its range. | The EXERR is the number of the operand that is out of range. The first operand is 0. For example, if EXERR = 4, then check the Decel Rate. | |
EXERR | MAS Operand | |||
0 | Axis | |||
1 | Motion Control | |||
2 | Stop Type | |||
3 | Change Decel | |||
4 | Decel Rate |
MAS Changes to Single Axis Status Bits
Motion Status Bits
If the Stop Type Is | Then | ||
---|---|---|---|
NOT All | The instruction clears the Motion Status bit for the motion process that you stopped. | ||
All | The instruction clears all Motion Status bits. | ||
Bit Name | State | Meaning | |
MoveStatus | FALSE | Axis is not Moving. | |
JogStatus | FALSE | Axis is not Jogging. | |
GearingStatus | FALSE | Axis is not Gearing. | |
HomingStatus | FALSE | Axis is not Homing. | |
StoppingStatus | TRUE | Axis is Stopping. | |
PositionCamStatus | FALSE | Axis is not Position Camming. | |
TimeCamStatus | FALSE | Axis is not Time Camming. | |
PositionCamPendingStatus | FALSE | Axis does not have a Position Cam Pending. | |
TimeCamPendingStatus | FALSE | Axis does not have a Time Cam Pending. | |
GearingLockStatus | FALSE | Axis is not in a Gear Locked condition. | |
PositionCamLockStatus | FALSE | Axis is not in a Cam Locked condition. | |
DirectVelocityControlStatus | FALSE | Axis is not under Direct Velocity Control. | |
DirectTorqueControlStatus | FALSE | Axis is not under Direct Torque Control. |
Provide Feedback