Array File-Misc Instructions
The file/miscellaneous instructions operate on arrays of data.
Available Instructions
Ladder Diagram
TIP:
STD
Function Block
Not available
Structured Text
If you want to: | Use this instruction: |
Perform arithmetic, logic, shift, and function operations on values in arrays | FAL |
Search for and compare values in arrays | FSC |
Copy the contents of one array into another array | COP |
Copy the value(s) in the Source to the Destination | CPS |
Fill an array with specific data | FLL |
Calculate the average of an array of values | AVE |
Sort one dimension of array data into ascending order | SRT |
Calculate the standard deviation of an array of values | STD |
Find the size of a dimension of an array | SIZE |
You can mix data types, but loss of accuracy and rounding error might occur and the instruction takes more time to execute. Check the S:V bit to see whether the result was truncated.
The
bold
data types indicate optimal data types. An instruction executes faster and requires less memory if all the operands of the instruction use the same optimal data type, typically DINT or REAL.Selecting Mode of Operation
For FAL and FSC instructions, the mode tells the controller how to distribute the array operation.
If you want to: | Select this mode: |
operate on all of the specified elements in an array before continuing on to the next instruction | All Mode |
distribute array operation over a number of scans enter the number of elements to operate on per scan (1-2147483647) | Numerical Mode |
manipulate one element of the array each time the rung-condition-in goes from false to true | Incremental Mode |
Provide Feedback