File Search and Compare (FSC)

This information applies to the
CompactLogix
5370,
ControlLogix
5570,
Compact GuardLogix
5370,
GuardLogix
5570,
Compact GuardLogix
5380,
CompactLogix
5380,
ControlLogix
5580,
GuardLogix
5580, and ControlLogix 5590 controllers. Controller differences are noted where applicable.
The FSC instruction compares values in an array, element by element.
Available Languages
Ladder Diagram
File Search and Compare (FSC) (1)_v31
Function Block
This instruction is not available in function block.
Structured Text
This instruction is not available in structured text.
Operands
IMPORTANT: Unexpected operation may occur if:
  • Output tag operands are overwritten.
  • Members of a structure operand are overwritten.
  • Except when specified, structure operands are shared by multiple instructions.
There are data conversion rules for mixing numeric data types within an instruction. See Data conversions.
Ladder Diagram
Operand
Data Type
CompactLogix
5370,
ControlLogix
5570,
Compact GuardLogix
5370, and
GuardLogix
5570 controllers
Data Type
CompactLogix
5380,
ControlLogix
5580,
Compact GuardLogix
5380,
GuardLogix
5580, and ControlLogix 5590 controllers
Format
Description
Control
CONTROL
CONTROL
Tag
Control structure for the operation
Length
DINT
DINT
Immediate
This represents the CONTROL structure .LEN
Position
DINT
DINT
Immediate
This represents the CONTROL structure .POS
Mode
DINT
DINT
Immediate
Shows how to distribute the operation.
Select INC, ALL, or enter number in the range of 1 to 2147483647
Expression
SINT
INT
DINT
REAL
STRING
SINT
INT
DINT
LINT
USINT
UINT
UDINT
ULINT
REAL
LREAL
String type
Immediate
Tag
An expression consisting of tags and/or immediate values separated by operators
Length and Position (corresponding to .LEN and .POS in the control tag) are pseudo-operands. For details, see Pseudo-operand initialization.
CONTROL Structure
Mnemonic
Data Type
Description
.EN
BOOL
The enable bit indicates the FSC instruction is enabled.
.DN
BOOL
The done bit is set when the instruction has operated on the last element (.POS = .LEN).
.ER
BOOL
The error bit is not modified.
.IN
BOOL
The inhibit bit indicates the FSC instruction detected a true comparison. You must clear this bit to continue the search operation.
.FD
BOOL
The found bit indicates the FSC instruction detected a true comparison.
.LEN
DINT
The length specifies the number of elements in the array on which the instruction operates.
.POS
DINT
The position contains the position of the current element that the instruction is accessing.
Description
When the EnableIn of the FSC instruction transitions from false to true, the expression is evaluated over the specified mode of iteration.
If the evaluation result is true, the instruction sets the .FD bit, and the .POS value reflects the array position where the instruction found the true comparison. The instruction sets the .IN bit to prevent further iteration.
Select Mode of Operation
For FSC instructions, the mode tells the controller how to distribute the array operation.
If you want to:
Select this mode:
Operate on all of the specified elements in an array before continuing on to the next instruction.
All
Distribute array operation over a number of scans.
Enter the number of elements to operate on per scan (1-2147483647).
Numerical
Manipulate one element of the array each time the EnableIn goes from false to true.
Incremental
All Mode
In All mode, all the specified elements in the array are operated on before continuing on to the next instruction. The operation begins when the instruction’s EnableIn goes from false to true. The position (.POS) value in the control structure points to the element in the array that the instruction is currently using. Operation stops under two conditions. When the .POS value equals or exceeds the .LEN value, AND when the expression evaluates to true.
File Search and Compare (FSC) (2)
The following timing diagram shows the relationship between status bits and instruction operation. When the instruction execution is complete, the .DN bit is true. The .DN bit, the .EN bit, and the .POS value are cleared when the EnableIn is false. Only then can another execution of the instruction be triggered by a false-to-true transition of EnableIn.
All Mode_2_v31
Numerical Mode
Numerical mode distributes the array operation over a number of scans. This mode is useful when working with non-time-critical data or large amounts of data. You enter the number of elements to operate on for each scan, which keeps scan time shorter.
Execution is triggered when the EnableIn goes from false to true. Once triggered, the instruction is executed each time it is scanned for the number of scans necessary to complete operating on the entire array. Once triggered, EnableIn can change repeatedly without interrupting execution of the instruction.
Numerical Mode
Avoid using the results of a file instruction operating in numerical mode until the .DN or .IN bit is true.
The following timing diagram shows the relationship between status bits and instruction operation. When the instruction execution is complete, the .DN bit is true.
FSC_Numerical Mode
If the EnableIn is true at completion, the .EN and .DN bit are true until the EnableIn goes false. When the EnableIn goes false, these bits are cleared and the .POS value is cleared.
If the EnableIn is false at completion, the .EN bit is cleared immediately. One scan after the .EN bit is cleared, the .DN bit and the .POS value are cleared.
Incremental Mode
Incremental mode manipulates one element of the array each time the instruction’s EnableIn goes from false to true.
FSC_Incremental Mode
The following timing diagram shows the relationship between status bits and instruction operation. Execution occurs only in a scan in which the EnableIn goes from false to true. Each time this occurs, only one element of the array is manipulated. If the EnableIn remains true for more than one scan, the instruction only executes during the first scan.
Incremental Mode_2
The .EN bit is set when rung-condition-in is true. The .DN bit is set when the last element in the array has been manipulated. When the last element has been manipulated and the rung-condition-in goes false, the .EN bit, the .DN bit, and the .POS value are cleared.
The difference between incremental mode and numerical mode at a rate of one element per scan is:
Numerical mode with any number of elements per scan requires only one false-to-true transition of the EnableIn to start execution. The instruction continues to execute the specified number of elements each scan until completion regardless of the state of the EnableIn.
Incremental mode requires the EnableIn to change from false to true to manipulate one element in the array.
Format expressions
For each operator that you use in an expression, you must provide one or two operands (tags or immediate values). Use the following table to format operators and operands within an expression.
For operators that operate on:
Use this format:
Example
One operand
operator(operand)
ABS(tag)
Two operands
operand_a operator operand_b
tag_b + 5
tag_c AND tag_d
(tag_e**2) MOD (tag_f / tag_g)
Determine the order of operation
The operations you write into the expression are performed by the instruction in a prescribed order, not necessarily the order you write them. You can override the order of operation by grouping terms within parentheses, forcing the instruction to perform an operation within the parentheses ahead of other operations.
Operations of equal order are performed from left to right.
Order
Operation
1
( )
2
ABS, ACOS, ASIN, ATAN, COS, DEG, BCD_TO, LN, LOG, RAD, SIN, SQRT, TAN, TO_BCD, TRUNC
3
**
4
- (negate), NOT, !
5
*, /, MOD
6
- (subtract), +
7
AND
8
XOR
9
OR
10
<, <=, >, >=, =, <>
11
&&
12
^^
13
||
Use strings in an expression
To use strings of ASCII characters in an expression, follow these guidelines:
An expression lets you compare two string tags.
You cannot enter ASCII characters directly into the expression.
Only the following operands are permitted:
Operator
Description
=
Equal
<
Less than
<=
Less than or equal
>
Greater than
>=
Greater than or equal
<>
Not equal
Strings are equal if their characters match.
ASCII characters are case-sensitive. Uppercase A ($41) is not equal to lowercase a ($61).
The hexadecimal values of the characters determine if one string is less than or greater than another string.
When the two strings are sorted as in a telephone directory, the order of the strings determine which one is greater.
FSC_use strings in an expression
Affects Math Status Flags
Controllers
Affects Math Status Flags
CompactLogix
5380,
ControlLogix
5580,
Compact GuardLogix
5380,
GuardLogix
5580, and ControlLogix 5590 controllers
No
CompactLogix
5370,
ControlLogix
5570,
Compact GuardLogix
5370, and
GuardLogix
5570 controllers
Yes
Major/Minor Faults
A major fault will occur if:
Fault type
Fault code
.POS < 0 or .LEN < 0
4
21
See Common Attributes for operand related faults. See Index Through Arrays for array-indexing faults.
Execution
Ladder Diagram
Condition / State
Action Taken
Prescan
N/A
Rung-condition-in is false
See FSC Flow Chart (Rung-condition-out is False)
Rung-condition-in is true
See FSC Flow Chart (Rung-condition-out is True)
Postscan
N/A
FSC Flow Chart (Rung-condition-out is False)
FSC Flow Chart EnableIn is False
FSC Flow Chart (Rung-condition-out is True)
FSC Flow Chart EnableIn is True
FSC Flow Chart (FSC Common Subflow)
FSC Flow Chart (FSC Common Subflow)
FSC Flow Chart (FSC Common Exception Subflow)
FSC Flow Chart FSC Common Exception Subflow
Examples
Example 1
Search between two DINT arrays for elements that are not equal.
Ladder Diagram
File Search and Compare (FSC)_Example1_v31
When enabled, the FSC instruction compares each of the first 10 elements in array_1 to the corresponding elements in array_2. When an element is found that is not equal, the FD and IN bits are set. The POS identifies the location of the not equal elements. Clear the IN bit to search the rest of the array.
FSC_example clear the bit
Example 2
Search for a string within a STRING array.
When enabled, the FSC instruction compares characters in code to 10 elements in code_table.
When a string in code_table is found that matches code, the FD and IN bits are set. The POS identifies the location of the matching strings. Clear the IN bit to search the rest of the array.
File Search and Compare (FSC)_Example3_v31
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal