Size In Elements (SIZE)

This information applies to the
Compact GuardLogix
5370,
ControlLogix
5570,
Compact GuardLogix
5370,
GuardLogix
5570,
Compact GuardLogix
5380,
ControlLogix
5580, and ControlLogix 5590 controllers.
The SIZE instruction finds the number of elements (size) in the designated dimension of the Source array or string operand and places the result in the Size operand. The instruction finds the size of one dimension of an array.
The instruction operates on:
  • Arrays
  • Arrays in a structure
  • Arrays that are part of a larger array
  • String tags
Available Languages
Ladder Diagram
RSL5K_SIZE Ladder Diagram_v31
Function Block
This instruction is not available in function block.
Structured Text
SIZE(Source,Dimtovary,Size);
Operands
IMPORTANT: Unexpected operation may occur if:
  • Output tag operands are overwritten.
  • Members of a structure operand are overwritten.
  • Except when specified, structure operands are shared by multiple instructions.
There are data conversion rules for mixing numeric data types within an instruction. See Data Conversions.
Ladder Diagram
Operand
Data Type
CompactLogix
5370,
ControlLogix
5570,
Compact GuardLogix
5370, and
GuardLogix
5570 controllers
Data Type
CompactLogix
5380,
ControlLogix
5580,
Compact GuardLogix
5380,
GuardLogix
5580, and ControlLogix 5590 controllers
Format
Description
Source
SINT
INT
DINT
REAL
structure
String type
BOOL
SINT
INT
DINT
REAL
LINT
USINT
UINT
UDINT
ULINT
LREAL
structure
String type
TIME
TIME32
LTIME
DT
LDT
Array tag
First element of the array on which the instruction is to operate
Tags that are not array are not accepted during verification
Dimension to Vary
DINT
DINT
immediate
(0, 1, 2)
Dimension to use:
For the size of:
Enter:
first dimension
0
second dimension
1
third dimension
2
Size
SINT
INT
DINT
REAL
SINT
INT
DINT
REAL
tag
Tag to store the number of elements in the specified dimension of the array
See Structured Text Syntax for more information on the syntax of expressions within structured text.
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See Index Through Arrays for array-indexing faults.
Execution
Ladder Diagram
Condition/State
Action Taken
Prescan
N/A
Rung-condition-in is false
Set Rung-condition-out to Rung-condition-in.
Rung-condition-in is true
Set Rung-condition-out to Rung-condition-in.
The instruction executes.
Postscan
N/A
Structured Text
Condition/State
Action Taken
Prescan
See Prescan in the Ladder Diagram table
Normal execution
See rung-condition-in is true in Ladder Diagram table.
Postscan
See Postscan in the Ladder Diagram table.
Examples
Example 1
Find the number of elements in dimension 0 (first dimension) of array_a. Store the size in array_a_size. In this example, dimension 0 of array_a has 10 elements.
Ladder Diagram
RSL5K_SIZE Ladder Diagram Example 1_v31
Structured Text
SIZE(array_a,0,array_a_size);
Example 2
Find the number of elements in the DATA member of string_1, which is a string. Stores the size in string_1_size.
In this example, the DATA member of string_1 has 82 elements. The string uses the default STRING data type. Since each element holds one character, string_1 can contain up to 82 characters.
Ladder Diagram
RSL5K_SIZE Ladder Diagram Example 2_v31
Structured Text
SIZE(string_1.DATA[0],0,string_1_size);
Example 3
String_a is an array of string structures. The SIZE instruction finds the number of elements in the DATA member of the string structure and stores the size in data_size_a.
In this example, the DATA member has 24 elements. The string structure has a user-specified length of 24.
Ladder Diagram
RSL5K_SIZE Ladder Diagram Example 3_v31
Structured Text
SIZE(string_a.[0].DATA[0],0,data_size_a);
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal