Add display objects

Different display objects (symbols) can be added to a library object to enable those displays to be used in HMI displays created using
FactoryTalk®
View Studio.
To add
FactoryTalk View
content to a library object
  1. Right-click the library object in the
    Library Content
    column and select
    Add Section > FT View
    . An
    FT View
    folder, with subfolders for
    Substitutions
    ,
    SE Symbols
    ,
    SE VBA Items
    , and
    ME Symbols
    , is added to the library object.
  2. Add a symbol to a library object. Repeat this process for all symbols needed for the library object:
    1. Right-click the
      SE Symbols
      or
      ME Symbols
      folder and select
      Add
      . The Symbol Builder dialog box opens.
    2. In
      Select Display Export File
      , enter the file location for the exported
      FactoryTalk View
      Symbol file and then press
      Enter
      or click the ellipsis (...) button to open
      Select a Display Export File
      dialog and navigate to the file, and then click
      Open
      . The symbols contained in the file are added to the
      Select Root Node/s of Symbol
      list.
    3. In the
      Select Root Node/s of Symbol
      list, select the symbol or group to import.
    4. (optional) In the
      Select Substitutions to Apply
      list, clear any substitutions that should not be applied.
      TIP:
      In a typical application, it is not necessary to clear any of the items in the
      Select Substitutions to Apply
      list.
    5. Click
      OK
      to import the symbol.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal