Symbol Builder dialog box
How do I open the Symbol Builder dialog box?
- In theLibrary Contentcolumn, expand theFT Viewsection, then click theSE SymbolsorME Symbolsfolder to select it.
- Right-click the folder and selectAdd. TheSymbol Builderwindow opens.
The
Symbol Builder
is used to configure how a display object is added to a library object. This table describes the configuration settings in the
Symbol Builder
dialog box.Setting | Type | Description |
|---|---|---|
Select Display Export File | Text entry or browse | The name of the exported FactoryTalk View graphics file that holds the symbols to import.Use the ellipsis (...) button to browse to the file location. |
Select Root Node/s of Symbol | List | A list of all symbols in the file. Symbols can be selected individually or as a group. However, only one symbol or group can be selected for each import. |
Select Substitutions to Apply | Checkboxes | When selected, apply substitutions for symbol attributes. There are two types of substitutions:
|
Provide Feedback