FT View substitutions

After adding a
FactoryTalk View
(
FT View
) section to the
Library Content
pane, configure substitutions and symbols for the objects.
Substitutions are used to quickly update
FactoryTalk View
objects with different text and other display objects as needed by an application. Substitutions can be created from the
Substitutions
property pane or from a symbol property pane. When substitutions are created from the symbol property pane, they are applied to that element immediately. When a substitution is created in the
Substitutions
property pane, it is not applied to an element immediately, but is available to be applied when the symbol is updated.
The
Substitutions
node under the
FT View
node in the
Library Content
pane displays a list of substitutions in the
Properties
pane. Substitutions can be added, edited, deleted or moved up and down from this view. None of these changes will be implemented into the displays though until they are updated.
Substitutions configured in
Library Object Manager
are not stored as decoration to the original data, but are applied into the original data. This means adding, removing, or editing a substitution can result in erroneous changes to the original data.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal